Hi,
I am trying to implement the people counting and tracking using mmWave radar sensor with sub-1 GHz reference design. Initially, there was an issue with the SDK version and its compatibility with LAUNCHXL-CC1352R1 Rev. E. So I followed the corrections made in the following thread:
After this I was successful in configuring the collector and sensor CC13251R devices without connecting the sensor to the Mmwaveic boost and also applied the patch files provided in the above mentioned thread.
As mentioned in the reference design document section 3.1.2.4 I was successful in building both the sensor and collector projects.
Are we supposed to re-flash the collector and sensor nodes after building the firmware? As there is no instructions in the design file to build the firmware again.
Regards,
Vandana