Hello,
are there any news to this thread: https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/964132/cc1310-maximum-number-of-connected-devices-in-wm-bus-data-collector-mode/3567393#3567393
I am highly interested in getting a number for the maximum of "installed" meters in the collector.
In the older thread the last answer is:
I got some additional information from the developers in addition to my old reply. In the uni-directional case, you should be able to increase the number up to the point that you run out of FLASH/RAM. I do not know the exact number but more then 16.
Can anybody estimate how much meters can be installed until we run out of FLASH/RAM?
An exact number would be nice, otherwise I need to know at least a space like 20, 50, 100, 200 ...
Best regards
SB