Other Parts Discussed in Thread: CC1310, CC1312R, CC1350
Hi,
We are in charge to create for new system RF proprietary network. Our goal is to be able to add maximum of 50 devices. We need to use ISM band (868/915) due to RF coverage requirements. As far as we read the radio module datasheet, there are several modes of operation, 802.15.4 and proprietary radio (the second seems best for our purposes). The system is telemetry system and each monitored device should send ~130bytes payload each 100mS, also some individual and broadcast commands should be received from the devices. The data rate (per device) is ~ 10*130 = 1300 bytes, total rate is ~50 * 1300 = 65KB/s
For this purpose we need to implement "Network like" simple Media Access Control. We can have single CC1310, acting as a network concentrator (similar to WiFi Access Point).
Do you have some recommendations, based on your experience if this should be possible to achieve, using the CC1310 proprietary radio commands, and if you can recommend how it will be best to create the media access level for collision avoidance - ether based on carrier detection before sending from each device, or hard network synchronization from single "master" device in the network.
Our additional goals are:
- We want to have address assignment, similar to the DHCP - the central device to detect how many clients are connected (for 1-2 seconds time for detection per new device) and give addresses. This task will be hardly achieved if there is single master, which to synchorize all the traffic. From the other hand, we do not have any experience with the CC1310 radio possibilities and any conceptual advice what we can read about will be highly useful for us.
Regards
Dimitar