Other Parts Discussed in Thread: CC1310
Dear Community,
Because CC1310 was out of stock I decided to switch to the CC1312R for a small batch which is an overkill and expensive for the purpose but at least was available.
I checked if there was any necessary modification and found that the only component is the 24MHz crystal which should be replaced with a 48MHz one.
I expected some minor modifications will be necessary in the firmware, but I failed at the very first step.
To try if everything is fine I launched Smart RF Studio with 2 instances of the new CC1312R connected. Everything went smooth, the boards could communicate with each other.
Then I tried one CC1310 and one CC1312R in pair and couldn't find any combination of settings where the two could communicate.
Is there anyone out there who can confirm if there is any chance to make it work or the product is not compatible.
Thanks