Other Parts Discussed in Thread: CC1310
Hey guys,
In the ARIB STD-T108 the output power is limited to 20mW (=13dBm). We are currently using the sensor/collector example for CC1310 SDK3.1 and CC1352R1 SDK3.1, respectively. Hence we set the output power in the respective config.h files.
Since we do not have the equipment to test our settings and since in SmartRF Studio only the values 14, 12.5, 12dBm aso are available.
I was wondering if can simply set
#define CONFIG_TRANSMIT_POWER 13
and
CCFG_FORCE_VDDR_HH == 0 (in respective opts-file)
or can I only use the values available in SmartRF Studio?
What are the available dBm values I can set for CC1352R1 config file?
Best wishes
Slev1n