Hi radio champs,
The CC1120 is used here as a 169MHz transceiver in a radio system - In reception the overall radio system (CC1120, MCU, TCXO, LNA, and the switch in the Skyworks PA) consumes around 30mA for a -121dBm sensitivity.
The same CC1120 radio module is evaluated for a repeater use case but the corresponding Rx consumption is too high.
Does it exist a CC1120 RX mode consuming less power? A loss in sensitivity could be acceptable in this application if that helps to lower the consumption.
Would the SNIFF mode use could be an option ?
Thank you!
Best regards,
Guillaume