This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: EnergyTrace Fails on CC1310

Part Number: CC1310
Other Parts Discussed in Thread: ENERGYTRACE

Hi,

I'm attempting to use the EnergyTrace Feature on Code Composer v8.3.1 using a CC1310 launch pad to analyze the current consumption of another, custom board using a CC1310F128. I've setup the launchpad as per the SWRA478D Application Report, with the EnergyTrace configurations as set below, with the difference being the 2-pin cJTAG cable going from the launch pad's XDS110 connector to the custom board.

Upon trying to start the EnergyTrace collection, the operation ends immediately with the message 'Stream Closed.  The data shows a time of 0 sec with an Energy of 0.000 mJ. I can manage to flash and debug the CC1310 under test, so I can't see this being an issue with the XDS110 simulator on the launch pad. What could be causing this?