This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: Simplelink SDK 5.30 and TI 15.4 stack fixed issues

Part Number: CC1352P

Hi team,

where can I get more information about the following issues that are fixed in Simplelink SDK 5.30 in the 15.4 stack? (list from https://software-dl.ti.com/simplelink/esd/simplelink_cc13xx_cc26xx_sdk/5.30.01.01/exports/docs/ti154stack/release_notes_ti154stack_4_30_00_00.html)

TI154STACK-3920         Reduce sync loss at high reporting intervals through start frame delimiter detection

TI154STACK-3919         Fix issue in which RSSI threshold MAC PIB not used for CSMA-enabled sub-G PHYs

TI154STACK-3918         Decrease MAC receiver max saturation to a reasonable level for good link indication

TI154STACK-3822         Fix issue in which device fails during high traffic loads due to OsalPort timers not cleared

Are the fixes in the closed-source part of the stack or are there specific code changes I can view?

Thanks and best regards,

hkr

  • Hi hkr,

    Unfortunately, this is the only information that it is available for the customers.

    I checked and the top three issues correspond to the low MAC. But the last issue relates to the OsalPort timers, so it should be possible to look for the changes between the SDK releases.

    BR,
    Andres