Other Parts Discussed in Thread: SYSCONFIG
Hi! I´m learning how to use Sensor Controller Studio with SimpleLink Academy tutorials with CC1352R1 LACUNHXL and CC1352-LPSTK. I am doing "Project from Scratch" tutorial and i have two doubts.
1) In I/O Configuration it says I have to comment on code lines from the file "CC1352R1_LAUNCHXL.c" but either I can't find the file or it's missing for some reason. I attached two images, the first one is a screenshot of my project and the second one is the example the tutorial provides.
2)I followed every step of the tutorial without having configured the file mentioned in point 1. When I build the project I get an error which is shown in the third image. It says the "Board_GPIO_RLED" variable is undefined so I don't know if I missed a step from the tutorial in which I had to define this variable or if this problem is related to the file from point 1.
Image 1:
Image 2:
Image 3:
Best Regards,
William