How to read the values from 'MAC IEEE 802.15.4 Address' registers in FCFG?
I tried:uint32_t mac_addr_lsb = HWREG(FCFG1_BASE + MAC_15_4_0);
uint32_t mac_addr_msb = HWREG(FCFG1_BASE + MAC_15_4_1);
// And:
uint32_t mac_addr_lsb = HWREG(FCFG1_BASE + FCFG1_O_MAC_15_4_0);
uint32_t mac_addr_msb = HWREG(FCFG1_BASE + FCFG1_O_MAC_15_4_1);
"#20 identifier "MAC_15_4_0" is undefined" and so on.
The example from where i try to read them is rfWakeOnRadioRx.
I guess i need to add some header, but what?
I've tried to search a header locally where these would be defined.
I'm new to TI. Using CCS 11.1.0.00011 on Windows 10.
Cheers