Other Parts Discussed in Thread: WI-SUN, CC1312R7, SYSCONFIG,
Hello,
I try to join the Wi-SUN network set up by the border router example for CC1312R7 board with a custom board used as router. Here is my TI settings :
I receive frames from the border router so preamble and sync word are deteced. It means there is the good datarate, center frequency, channel(?) etc, so regulatory domain/Phymode seems to be correct. Is that right? I have doubts about data whitening, can an unmatched setting between nodes and BR prevent joining network without preventing my node to receive some frames? (wrong frames) I precise I can join the network with another TI board without issue so I am sure there is a setting mismatch between my custom router and the BR, but I can't figure out which one. I checked the network name several times.
Thank you for your help