Hi,
I am designing a radio product with CC1125 that will be compatible with a legacy protocol in FSK. Thus I am using the Transparent Serial Mode, which works as expected. Now I want to minimize the Adjacent Channel Power (ACP) and I have realized that the User's Guide (swru295e) is very brief when it comes to TX data filtering. By playing with register values however, I note that there is an impact on the modulation filter bandwidth from the Symbol Rate that I set (even though it is not doing any synchronizing in the Tranparent Serial Mode). There is also an impact from the UPSAMPLER_P value. Are these the parameters that I should play with?
Also, I see a not-so-clean spectrum around the carrier due to spurrs at kHz-offsets. Can I play with and optimize any register values for the Frequency Synthesizer to mitigate this?
Thank you.