Other Parts Discussed in Thread: WMBUS, CC1312R
Hi
while measuring RSSI vs time (Rx continuous), i observed that the RSSI reading for the LP-CC1312R7 get stuck after some time.
i.e. changing the signal level does not result in a change in RSSI, less than 10 minutes after pressing start continuous rx.
Is this a known bug for RF studio or a side effect of the lack of repeated internal RF calibration for the PLL / PLL unlock ?
The radio is configured to the following settings : 869.525 MHz, gfsk, 25 kHz deviation, 50 kb/s (i.e. wmbus mode C for EU, OTM)
We use a wmbus c-mode MTO setup to start and change the carrier and modulation parameters to match OTM settings.
when the measurement is running normally i get the following plots
During testing of the evaluation board vs temperature i have also observed the following :
During the temperature cycling from 85 degC to 0 degC, it was observed that, the frequency carrier drift by 1.8 kHz until the radio is stopped and restarted.