Hello Team,
Can you have a look at the following FW question please?
From our PCB production comes the request, if we could provide a "special" firmware, which does nothing else than boot the chip and outputs a permanent transmit signal at the antenna.
I am now in the awkward position that the firmware development for this chip is not in-house and we cannot develop anything special for it.
I know that you can set different radio modes like "Continuous Transmit unmodulated 868.0MHz" through the development boards.
I also know that there is code from TI like #rfCarrierWave.
But my question is, do you happen to have a ready firmware available that runs on the CC1310 and goes into a mode similar to "Continuous Transmit unmodulated 868.0MHz" right after boot?
Thank you,
Franz