Other Parts Discussed in Thread: CC1312R7, UNIFLASH, CC1312R
Hi,
My customer needs to migrate CC1312R1 to CC1312R7.
I know the two devices have different memory sizes and I did a guide to the customer.
My customer is using contiki-ng and this doesn't support R7.
But I thought the difference between the two devices is the memory size, so I just changed the memory map and it would work.
I changed memory map in cc13x2-cc26x2.lds and cc13x2-cc26x2.icf files.
And then I make image file and program using the uniflash. but it doesn't work.
The EVMs of the two devices is different, but I have confirmed that the pin map in the schematics are the same.
So I used the source of the cc1312r launchpad without any changes.
Is there anything I need to change?