Hello,
We need help finding a replacement crystal oscillator than the one recommended for use with the cc1200. As recommended in the CC1200EM design files we are using the 40MHz crystal, part # NX3225SA-40M-EXS00A-CS03880, to drive XOSC. The external load capacitors have also been kept as 15pF. Due to current shortages we are looking at direct drop-in alternates for the crystal oscillator.
ABM8-40.000MHZ-10-D1G-T has the same load capacitance and frequency tolerance as well as slightly better frequency stability. It however has a lower ESR compared to the original. Is this part suitable for replacement?
Thank you for your help recommending a replacement crystal oscillator.