HI,
I am using the CC1125 with a clipped Sine TCXO (Taitien part TYETBLSANF-40.000000).
This part has a low signal level output (approx 820mV pk-pk at ambient). As the temperature is reduced, the amplitude falls. At much below -10C the amplitude is less than the 800mV minimum specification for the CC1125. (It has also fallen out of the published spec of the Taitien part). But, this is one of the few TCXOs that are currently available from distribution.
I am experiencing issues whereby the CC1125 is not receiving this clock as the tempertaure falls. I do understand that I am going outside of the published spec.
Does anyone know of any means of increasing the sensitivity of the external clock input of the CC1125? Do any of the register settings affect this? (I know there are several XOSC registers with the description as 'reserved!')
Any help in this matter would be greatly appreciated.
Regards,
Ian