Other Parts Discussed in Thread: CC1312R, SYSCONFIG, CC1310
Hello,
I'm trying to use SmartRF studio 7 (2.25.0) to configure the CC1312R eval board to use the TXCO. I have proved an output by swapping across the hardware (though running the TCXO from VDDS rather than DIO30).
Page 26 here suggests that the TCXO settings are in 'device configuration' but I can't find that menu. The closest one only has an option to set the RF output between diff or single ended, but nothing on the input clock.
My aim is to produce a fixed frequency CW output with as little phase noise as possible. There is section 13.3 here covering phase noise, but this is on the code export output - is there any information as to how to do this using the override editor for individual registers?