Part Number: CC1352P
Other Parts Discussed in Thread: , SYSCONFIG
A customer is evaluating the 500kbps GFSK PHY for wireless microphone application. A difference has been noticed between CC1352P and CC1352P7 using the same PHY: the Rx bandwidth for this PHY setting is 1150kHz on CC1352P, while on CC1352P7 it is 622kHz.
1. Why is the Rx bandwidth different on these two devices? Is there a hardware difference/limit?
2. Can I use 622kHz Rx bandwidth on CC1352P by manually changing the RF setup command? I want to find out the maximum distance of the 500k PHY, theoretically a larger Rx bandwidth will decrease the distance, is that correct?
3. Is the 500k GFSK PHY recommended for wireless mic application in general? The customer's requirement is >400kbps data rate and >200m range, is it feasible?
Best regards,
Shuyang