This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1310: Project blocking problem.

Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: CC1310

Hi team,

Here's the request from the customer:

Customer is confused that the project would block when operate floating point operations.

The snapshot is shown in the following figure:

Could you help check this case? Thanks.

Best Regards,                                                            

Nick    

  • Resolution of the screenshot is so bad, so I am not able to read what it says. 

    Please take the empty project on the latest CC1310 SDK and modify it to generate the problem that the customer is seeing, and I will take a look at it.

    Share the modified empty.c as a file or use the "insert code" option and paste in the code there so I can copy and paste it in my project.

    Siri

  • Hi Siri,

    I will ask customer for further file.

    The HD snapshot is shown in the following figure:

    Best Regards,                                                            

    Nick    

  • I suppose you have issue to print float value and you can refer to the solution in e2e.ti.com/.../2980488