Hi, support team
My customer has the questions as follow:
Question 1: The test current uses 3.3V power supply, parameter reference file SWRA528.pdf to 3.20x1CC7, the power supply current of 3.3V is 38mA, and the maximum emission current is 125mA, which is deviated from the document.
Question 2. The transmitter board adopts CC1310 +PA design parameters refer TO 528.pdf TO 3.20x1CC7, the receiver board adopts CC1310 DEMO design, test band 433.92032MHZ 625 LLR receiver board uses SmartRF 7 test, There are 9671 test results, including Received OK 9224,Received NOT OK 231, and Packet Error Rate is 2.4%. The Packet Error Rate is relatively high. What is the cause of this? Do you refer to the documentation
Thanks so much.
Best regards,
Yuki