Other Parts Discussed in Thread: WMBUS,
I'm working on a project based on EasyLinkEcho (RX/TX) example (SimpleLink CC13x0 SDK v4.20.02.07 in CCS 12.0.0.00009).
In parallel I'm using wMBus stack (wmbus-cc13xx-rtos-2.0.0 in CCS 8.1.0.00011) on a different device set (also CC1310).
I'd like to create a collector device being capable of receiving both EasyLink based messages and wMBus telegrams (C mode & probably T mode).
I adapted smartrf_settings.c in EasyLink based on the C mode wMBus smartrf_settings (sf_cc13xx_868_95.c) but some parameters had to be excluded to be able to build the EasyLink based project in CCS 12.
#include <ti/devices/DeviceFamily.h> #include DeviceFamily_constructPath(driverlib/rf_mailbox.h) #include DeviceFamily_constructPath(driverlib/rf_common_cmd.h) #include DeviceFamily_constructPath(driverlib/rf_prop_cmd.h) #include <ti/drivers/rf/RF.h> #include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_genfsk.h) #include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_genfsk.h) #include "smartrf_settings.h" uint32_t txShapeCMode[] = {0x00000000, 0x00000000, 0x00000000, 0x440F0200, 0xD9D8CA96, 0xD9D9D9D9}; // TI-RTOS RF Mode Object RF_Mode RF_prop = { .rfMode = RF_MODE_PROPRIETARY_SUB_1, .cpePatchFxn = &rf_patch_cpe_genfsk, .mcePatchFxn = 0, .rfePatchFxn = &rf_patch_rfe_genfsk, }; // Overrides for CMD_PROP_RADIO_DIV_SETUP uint32_t pOverrides[] = { //Run the MCE and RFE patches MCE_RFE_OVERRIDE(1,0,0,1,0,0), // override_synth_prop_863_930_div5.xml // Synth: Set recommended RTRIM to 7 HW_REG_OVERRIDE(0x4038,0x0037), // Synth: Set Fref to 4 MHz (uint32_t)0x000684A3, // Synth: Configure fine calibration setting HW_REG_OVERRIDE(0x4020,0x7F00), // Synth: Configure fine calibration setting HW_REG_OVERRIDE(0x4064,0x0040), // Synth: Configure fine calibration setting (uint32_t)0xB1070503, // Synth: Configure fine calibration setting (uint32_t)0x05330523, // Synth: Set loop bandwidth after lock to 20 kHz (uint32_t)0x0A480583, // Synth: Set loop bandwidth after lock to 20 kHz (uint32_t)0x7AB80603, // Synth: Configure VCO LDO (in ADI1, set VCOLDOCFG=0x9F to use voltage input reference) ADI_REG_OVERRIDE(1,4,0x9F), // Synth: Configure synth LDO (in ADI1, set SLDOCTL0.COMP_CAP=1) ADI_HALFREG_OVERRIDE(1,7,0x4,0x4), // Synth: Use 24 MHz XOSC as synth clock, enable extra PLL filtering (uint32_t)0x02010403, // Synth: Configure extra PLL filtering (uint32_t)0x00108463, // Synth: Increase synth programming timeout (0x04B0 RAT ticks = 300 us) (uint32_t)0x04B00243, // override_phy_rx_aaf_bw_0xd.xml // Rx: Set anti-aliasing filter bandwidth to 0xD (in ADI0, set IFAMPCTL3[7:4]=0xD) ADI_HALFREG_OVERRIDE(0,61,0xF,0xD), // override_phy_gfsk_rx.xml // Rx: Set LNA bias current trim offset to 3 (uint32_t)0x00038883, // Rx: Freeze RSSI on sync found event HW_REG_OVERRIDE(0x6084,0x35F1), // override_phy_gfsk_pa_ramp_agc_reflevel_0x2e.xml // Tx: Configure PA ramping setting and set AGC reference level to 0x2E HW_REG_OVERRIDE(0x6088,0x082E), // Tx: Configure PA ramping setting and set AGC settle wait = (0x7+1)*2 = 16 samples HW_REG_OVERRIDE(0x608C,0x0407), // override_phy_rx_rssi_offset_5db.xml // Rx: Set RSSI offset to adjust reported RSSI by +5 dB (uint32_t)0x00FB88A3, // TX power override // Tx: Set PA trim to max (in ADI0, set PACTL0=0xF8) ADI_REG_OVERRIDE(0,12,0xF8), // AGC winsize 2 samples HW_REG_OVERRIDE(0x6064,0x1101), // CS threshold to �107 dBm HW_REG_OVERRIDE(0x6090,0xA095), // Let the patch control the correlator setting (uint32_t)0x00048103, // Clear state in internal radio register due to frequency change HW_REG_OVERRIDE(0x51F8,0x0000), HW_REG_OVERRIDE(0x52B4, 0x4000), // Set divider bias to disabled HW32_ARRAY_OVERRIDE(0x405C,1), (uint32_t)0x18000200, // TX shape in T-mode //0xC0040031, //(uint32_t)&txShapeTMode[0], // TX shape in C-mode 0xC0040031, (uint32_t)&txShapeCMode[0], (uint32_t)0xFFFFFFFF, }; // CMD_PROP_RADIO_DIV_SETUP rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup = { .commandNo = 0x3807, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .modulation.modType = 0x0, .modulation.deviation = 0xB4, // T-Mode: 0xC8, C-Mode: 0xB4. /* According to swra522d we have to change the deviation setting for C-meters */ .symbolRate.preScale = 0xC, .symbolRate.rateWord = 0xCCCD, .rxBw = 0x27, .preamConf.nPreamBytes = 0x4, .preamConf.preamMode = 0x0, .formatConf.nSwBits = 0x10, .formatConf.bBitReversal = 0x0, .formatConf.bMsbFirst = 0x1, .formatConf.fecMode = 0x0, .formatConf.whitenMode = 0x0, .config.frontEndMode = 0x0, .config.biasMode = 0x1, .config.analogCfgMode = 0x0, .config.bNoFsPowerUp = 0x0, .pRegOverride = pOverrides, .txPower = 0xA73F, .centerFreq = 0x0364, .intFreq = 0x8000, .loDivider = 0x05, }; // CMD_FS rfc_CMD_FS_t RF_cmdFs = { .commandNo = 0x0803, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .frequency = 0x0364, .fractFreq = 0xF334, .synthConf.bTxMode = 0x0, .synthConf.refFreq = 0x0, .__dummy0 = 0x00, .__dummy1 = 0x00, .__dummy2 = 0x00, .__dummy3 = 0x0000, }; // CMD_PROP_TX rfc_CMD_PROP_TX_t RF_cmdPropTx = { .commandNo = 0x3803, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .pktConf.bFsOff = 0x0, .pktConf.bUseCrc = 0x0, // .pktConf.bCrcIncSw = 0x0, // .pktConf.bCrcIncHdr = 0x0, // .numHdrBits = 0x00, .pktLen = 0x0000, // .startConf.bExtTxTrig = 0x0, // .startConf.inputMode = 0x0, // .startConf.source = 0x0, // .preTrigger.triggerType = 0x0, // .preTrigger.bEnaCmd = 0x0, // .preTrigger.triggerNo = 0x0, // .preTrigger.pastTrig = 0x0, // .preTime = 0x00000000, .syncWord = 0x0000543D, .pPkt = 0, /*INSERT APPLICABLE POINTER: (uint8_t*)&xxx */ }; // CMD_PROP_RX rfc_CMD_PROP_RX_t RF_cmdPropRx = { .commandNo = 0x3804, .status = 0x0000, .pNextOp = 0, /*INSERT APPLICABLE POINTER: (uint8_t*)&xxx */ .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .pktConf.bFsOff = 0x0, .pktConf.bRepeatOk = 0x0, .pktConf.bRepeatNok = 0x0, .pktConf.bUseCrc = 0x0, // .pktConf.bCrcIncSw = 0x0, // .pktConf.bCrcIncHdr = 0x0, .pktConf.endType = 0x0, .pktConf.filterOp = 0x0, .rxConf.bAutoFlushIgnored = 0x0, .rxConf.bAutoFlushCrcErr = 0x0, .rxConf.bIncludeHdr = 0x0, .rxConf.bIncludeCrc = 0x0, .rxConf.bAppendRssi = 0x0, .rxConf.bAppendTimestamp = 0x0, .rxConf.bAppendStatus = 0x0, .syncWord = 0x0000543D, // .syncWord1 = 0x00000000, .maxPktLen = 0x0000, // .hdrConf.numHdrBits = 0x0, // .hdrConf.lenPos = 0x0, // .hdrConf.numLenBits = 0x0, // .addrConf.addrType = 0x0, // .addrConf.addrSize = 0x0, // .addrConf.addrPos = 0x0, // .addrConf.numAddr = 0x0, // .lenOffset = 0x00, .endTrigger.triggerType = 0x0, .endTrigger.bEnaCmd = 0x0, .endTrigger.triggerNo = 0x0, .endTrigger.pastTrig = 0x0, .endTime = 0x00000000, // .pAddr = 0, /*INSERT APPLICABLE POINTER: (uint8_t*)&xxx */ .pQueue = 0, /*INSERT APPLICABLE POINTER: (dataQueue_t*)&xxx */ .pOutput = 0, /*INSERT APPLICABLE POINTER: (uint8_t*)&xxx */ };
However, the EasyLink receiver does not receive data from the wMBus "Meter" (wmbus stack for CC1310 with APL_CC13XX_Meter_T2_C2 and "wmbus_setMode(WMBUS_MODE_C2);" rather than the default "wmbus_setMode(WMBUS_MODE_T2);").
A test in advance based on a wMBus "Collector" (wmbus stack for CC1310 with Serial_CC13XX_Collector_C2) successfully receives the sent packages.
In SmartRF Studio 7 with continuous RX a spike (-20dBm) can be seen but no packet received there either.
SmartRF Settings:
Unfortunately I was not able to confirm my settings but found a statement that packets should be receivable here: how to configure Smart RF studio for T&C mode?
1) What settings should be used in SmartRF Studio to receive a packet sent from a wMBus device in C Mode (and/or T Mode)?
2) Is it possible to use EasyLink Abstraction layer ("EasyLink_receiveAsync") to receive wMBus (C Mode and/or T Mode) telegrams?
2.1) If yes, how can I achieve it?
2.2) If not, what could be possible solutions to use a simple RX/TX framework and wMBus in parallel on collector side (data can be processed on higher level later)?
Thanks in advance!