We need help to implement a WI-SUN network in the city of Quito, for this we require concentrators and repeaters, in order to have the monitoring of electricity meters of different brands. Therefore we have the following questions:
1.- There are concentrators that are capable of communicating with end nodes of different brands.
2.- The frames received by the concentrator can be redirected to its own server in order to be able to carry out data processing on its own and thus have its own monitoring software.
3.- You can have a signal range greater than 5 km
4.- They will be able to provide us with the electronic cards to make our own equipment as well as concentrators and repeaters.
5.- It will be possible for them to provide us with electronic cards to be able to assemble electricity meters.
6.-The last question would be about the capacity of the concentrators, what is the maximum capacity of the WI-SUN concentrators?
Thanking you for the attention given to this
Greetings.