Other Parts Discussed in Thread: UNIFLASH
Hello,
I'm having an issue with programming the CC1352P7 device with the Flash Programmer 2 version 1.8.2 (latest). I can connect to this device OK from Code Composer Version 12.0.0.9 as well with the recent upgrade (today) to version 12.1.0.7 ok. I want to use the Flash Programmer 2 to program the hex image that I would give to production which is the tool that they utilize to program these devices. The error I am getting is that it failed to enumerate XBAL devices. When I upgraded today to version 12.1.0.7 I noticed that it did an upgraded of my XDS110 device as well to emulation package 9.9.0.0.40 which I recall an upgrade similar when updating to CCS 12.0.0.9 previously (I don't recall the release at that time). I notice that the Flash Programmer 2 tool hasn't been upgrade in 2 years. What is causing this issue such that I cannot use the Flash Programmer 2 tool?
Thank you,
Shawn