Other Parts Discussed in Thread: CC1352R, SYSCONFIG
Hello,
I am trying to communicate via SPI. I have started with the SPI Master Example (spimaster_CC1312R1_LAUNCHXL_tirtos_ticlang) and tried to modify it so that it fit my needs. But I can't get it to work properly, the CS line get's deasserted after every byte. But I need the CS line low for the duration of the transaction. How do I achieve this?
The Waveform look like this.
Frame Format: SPI mode Polarity 0 Phase 1

But I need it like this:

Here: CS is low for the duration of the read operation (transaction?) And thats what I need.
I tried all spi frame formats:
- SPI mode Polarity 0 Phase 0
- SPI mode Polarity 0 Phase 1
- SPI mode Polarity 1 Phase 0
- SPI mode Polarity 1 Phase 1
- TI mode
- Micro-wire mode
with no success.
I am using:
- CCS 12
- TI RTOS
- CC1352R
- CC13x2 SDK
Thanks in advance and
Kind regards