Other Parts Discussed in Thread: CC1120, SIMPLELINK-CC13XX-CC26XX-SDK
Hi experts,
My customer wants CC1312 and CC1120 to communicate.
If the customer has the following specifications, the device can communicate normally.
・ Proprietary protocol
・ Packet Count: 150
Program : They refer to rfPaketTx and rfPaketRx and use CMD_PROP_TX and CMD_PROP_RX
However, in the case of the following specifications, the device cannot communicate.
・ Proprietary protocol
・Packet Count: Infinite
Program: They refer to rfPaketTx and rfPaketRx and use CMD_PROP_TX_ADV and CMD_PROP_RX_ADV
Now I have the following questions:
Q1
Can CC1312 and CC1120 communicate with Packet Count set to Infinite?
Also, do you have these sample programs for communicating?
Q2
Is there a sample code that can send and receive data with a packet count exceeding 255 bytes using two CC1312s?
Best regards,
Sasaki