Other Parts Discussed in Thread: CC1312R, ENERGYTRACE
Hi
I have testing sleep and low power I don't seem to be able to go below 0.9mA, I have been advise that there could be two issues one is the JTAG is running and the other is the 48MHz clock.
Also for a sanity check I used the empty SDK and that also is high at 0.58mA
Can anyone please show me how to disable the JTAG and use the 32K clock or point me towards examples example.
Regards
David