Other Parts Discussed in Thread: SYSCONFIG,
Hi,
I want to put some info (like TI OAD image hader), with size 0xA8 bytes, in front of my application code. In order to do this as a first step I just move Flash vector table to start of 0xA8 instead of 0x0 changing FLASH region in linker command file and Flash vector table start address in CCFG (using Sysconfig).
timerled_CC1312R1_CodeOffset_test.zipThe problem is that after my changes the prooject could run only on debuger after loading it to target (Run to main()). Not works without debuger and after "Board reset" with debuger (loops endlessly in UARTAutoBaud() ROM function).
I've recriated this with the "Timerled" example adding additional build configurations with "A8_CodeOffset" within its name.
timerled_CC1312R1_CodeOffset_test.zip
Could you tell me what I miss?
Regards,
Dimitar