Hi,
I'm trying to write code in SCS which loops through events A->B->C->A.
The trigger between A->B and B->C is with evhSetupGpioTrigger(0, AUX_IO_NAME, 0, EVH_GPIO_TRIG_ON_EDGE), which works fine.
I want to trigger the move from event C->A immediately (without depending on other GPIO triggers), I tried using evhSetupTimer0Trigger(0,1,0) but this could lead to a delay of up to 250 us as I understand.
Is there a better way to implement immediate transitions between events?