I wanted to update the SDK for my CC1310 TI-RTOS project. I was using the SimpleLink CC13x0 SDK (4.20.02.07) and needed some more GPIO ISR features which I found in the 6.40 (see here https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1195214/cc1310-passing-parameters-to-gpio-interrupts-other-than-the-index/4505438?tisearch=e2e-sitesearch&keymatch=%20user%3A551061#4505438)
But changing the SDK caused the RTOS project to not compile anymore:

Then I found:
"CC13x0 and CC2640R2 devices will continue to use their respective SDKs." in the description of the "SimpleLink CC13xx CC26xx SDK (6.40.00.13)" SDK.
Am I doing something wrong with the includepaths or is the CC1310 just not included in CC13xx??