Other Parts Discussed in Thread: SYSBIOS, WI-SUN,
Hi
UPDATE to update: Previous statement was wrong. It crashes with security disabled. However the exception *only* occurs if there is a running WiSun network with a border router. So if the network code does not see a network in the air, no exception occurs.
We are getting HWI exception in the above function (accordingt to the SP,LR,PC registers in the exceptionInfo)
How do we fix this?
Stack trace according to debugger:
Texas Instruments XDS110 USB Debug Probe/Cortex_M4_0 (Suspended)
macAllocTxBuffer() at mac_hl_patch.c:1 690 0x00048A76
macBuildCommonReq() at mac_hl_patch.c:2 739 0x00033B1E
macRadioSendEnhAck() at mac_radio_tx.c:1 179 0x0007B402
rxFcsIsr() at mac_rx.c:1 331 0x0001524A
rxPayloadIsr() at mac_rx.c:1 052 0x00015024
rxStartIsr() at mac_rx.c:0 0x0000B590
macRxFrameIsr() at mac_rx.c:400 0x0000B2FE
macRxCbSubG() at mac.c:0 0x00021E3C
macRxCb() at mac.c:546 0x00021E1C
RF_radioOpDoneCb() at RFCC26X2_multiMode.c:2 947 0x00039496
RF_fsmActiveState() at List.h:155 0x0000E9AC
ti_sysbios_knl_Swi_run() at Swi.c:185 0x0006994A
ti_sysbios_knl_Swi_restoreHwi() at Swi.c:440 0x0005538A
ti_sysbios_family_arm_m3_Hwi_doSwiRestore() at Hwi.c:1 754 0x0008A7FA
ti_sysbios_family_arm_m3_Hwi_dispatch + 0xb0 ()