Other Parts Discussed in Thread: CC1120, CC1175, CC1310, CC1125
Hi Team,
Our customer is considering the CC1120EM-420-470-RD for nanosatellite application and has some inquiries as follows:
Does the chip CC1120EM-420-470-RD can transmit data between nanosatellites to ground stations the distance between them is up to 400km with band frequency UHF from uplink and vhf of the downlink
- If yes, can add a bloc of amplifier signal between the chip CC1120EM-420-470-RD and antenna to achieve that the signal can propagate a long distance of 400km
- If yes, can use the transmitter and receiver with mode half duplex with a data rate is 4000kps?
- If yes, is better to add two blocs in the design of my own board once from the transceiver(CC1120EM-420-470-RD ) and the second from the receiver (CC1120EM-420-470-RD ) or use only once that can transmit and receiver in mode half duplex?
- Which kind of modulation should be used from carried data up to 400km?
- how can design and choose the right antenna for CC1120EM-420-470-RD that can transmit data up to 400km?
- which better to put in my own board of antenna SMA antenna or PCB antenna?
please send any documents from my questions and thank you for helping
Regards,
Danilo