Other Parts Discussed in Thread: CC1354P10, SYSCONFIG
Hi,
I have questions regarding rfEchoRX/TX demo project in the Simplelink cc13xx cc26xx SDK (v7.10.01.24) in CC1354P10-1 below.
C:\ti\simplelink_cc13xx_cc26xx_sdk_7_10_01_24\examples\rtos\LP_EM_CC1354P10_1\prop_rf\rfEchoRx
C:\ti\simplelink_cc13xx_cc26xx_sdk_7_10_01_24\examples\rtos\LP_EM_CC1354P10_1\prop_rf\rfEchoTx
- Do you have any documents for the wireless communication protocol stack used in this demo, especially for address management and routing at the network layer?
- Are the specifications up to the network link layer in the demo in accordance with IEEE 802.15.4?
From the RF stack of SYSCONFIG, we understand that the proprietary RF "50 kbps, 25 kHz Deviation, 2-GFSK, 100 kHz RX Bandwidth" is used up to the PHY layer.
We also understand that the data link layer is also set in the Link layer of Custom PHY setting.
However, we do not yet know the specifications for protocols at the higher layers.
Also, it appears that IEEE 802.15.4 is not selected in the default settings in the same setting bellow.

Best Regards,