Other Parts Discussed in Thread: CC1125,
Hello
We are using CC1125 for 12,5kHz narrow band application at 869,212MHz (Social Care under EN300-220), and using a 38,4MHz TCXO clock.
Supply voltage= 3,3V
Have found that CC1120 is nearly identical to CC1125, but only specified to using 32MHz crystal.
We have tried to replace a CC1125 by CC1120, and did keep the 38,4MHz TCXO clock.
I seems to work fine
Questions:
- For what reason are crystal frequency for CC1120 limited to 32MHz?
- What is the consequence of feeding a CC1120 by 38,4MHz from TCXO?
Regards Knud