Other Parts Discussed in Thread: CC1020
Hello there,
We are measuring sensitivity by sending a preamble from a signal generator. As soon as 10.000 Bits are correct (= alternating 0 or 1) a LED lights up. If one bit is wrong the LED turns off. We are using synchronous serial mode. We are trying to get the LED to stay on for at least 10 seconds. Our current sensitivity is at -103 dBm. This seems to be pretty high.
Is there a measurable difference in conducted sensitivity when changing the mode to using FIFOs?
Does RFStudio generate the best possible values for sensitivity or is it possible to get a better value by optimizing the parameters?
What Sensitivity values are expected when using 433MHz, 50kHz BW, 19200kBits Symbol Rate, 2-FSK?