This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R: Sensor Controller Studio Debugger execution task time out

Part Number: CC1312R


Hi,

I have a sensor controller task that waits for ADC readings to stabilize. It is an auto-calibration application repeated for 6 input settings controlled by an analogue switch via SPI.. The whole process can take up to 20 seconds.

Using the SC Studio task debugger I get an execution timeout (stuck) error and it all stops. The debugger is really useful for debugging the interface circuitry so I need to find a work around.

I have 2 questions:

  1. How long is the execution task debugger timeout?
  2. Is there an action that resets the timer?

Any help would be much appreciated,

Thanks