This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-CC1311P3: Can LP output frequencies besides 868-915MHz?

Part Number: LP-CC1311P3
Other Parts Discussed in Thread: CC1311P3

The user guide and quick-start guide isn't clear whether the launchpad can output frequencies besides 868MHz or 915MHz. The CC1311P3 is designed to operate in many other frequency bands so I am wondering if the launchpad can be used to output 400MHz if using the SMA connecter? Any information is appreciated!