Part Number: CC1310
Hello, Dears
We conducted communication distance testing using CC1310 in an underground garage environment, with a testing frequency of 433MHz. The data is as follows:
1. CC1310 does not use the TI 15.4 protocol stack and uses simple sending and receiving routines in the SDK to test communication distance, which can reach approximately 400m.
2. CC1310 uses the TI 15.4 protocol stack, and the communication testing distance is only 250m.
May I ask if your company's own testing data has been compared between those with and without protocol stacks?
Or, do you have any relevant experience or conclusion that the TI 15.4 protocol stack has an impact on the distance of 433MHz wireless communication?