This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101: Low power & long range (& low cost). LoRa replace

Part Number: CC1101
Other Parts Discussed in Thread: CC1190, CC1311R3, CC1311P3, CC1312R, CC1352R, CC1352P, CC1312R7, CC1352P7, CC1354R10

I have a product designed with LoRa and I'm wondering if we can switch to some SubGhz transceiver chip with the same or better specifications. And also have the Wake on Radio function filtering address before sending the interrupt to the main MCU.
I have used CC1101 in the past, but I don't know how it works at a very long range (several KM), and there is also not enough information on this topic, so I don't know if there is any bug compared to LoRa. There are also amplifiers to increase the range and for the gateway it can be an option because there are no power restrictions, but the final device must be ultra-low power.

Greetings