Other Parts Discussed in Thread: CC1101, CC1120
Hi.
I am completing a PCB design using this eval board as a reference. I would like to know if all the 47nF capacitors can be replaced with 100nF capacitors on the CC120RHBR? They look like they are just filtering DC levels. Will using 100nF X7R ceramic caps cause any misbehaviour? It seems odd that 47nF caps were needed for filtering, and not 100nF suggested. From a technical perspective, why 47nF?
Also,C61 is 220nF. Can I used a 1uF cermic cap instead?
This will be a high volume PCB of around 20,000+ units per annum initially and growing thereon. I want to reduce to the BOM item count as I am using 100nF caps and 1uF capc elsewhere on the PCB.
regards,
David.