[FAQ] SimpleLink Academy TI Wi-SUN FAN Linux Host Wfantund

The new SimpleLink Academy TI Wi-SUN FAN Linux Host Wfantund guides you through the network set-up using wfantund from the terminal and using the Wi-SUN WebApp. It introduces network testing methods using ping and iPerf. Finally, it teaches you how to connect an external DHCP server and an external authentication server to the wfantund interface.

Task 1: Setup and configuration of the embedded projects and wfantund.

Task 2: Network setup with the Wi-SUN web application.

Task 3: Network setup with the wfanctl terminal interface.

Task 4: Host to host UDP communication.

Task 5: Network throughput test using iPerf.

Task 6: External DHCPv6 server using dnsmasq.

Task 7: External authentication server using FreeRADIUS.

Check it out here!