This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1354P10: Address set and check in proprietary radio command structures

Part Number: CC1354P10
Other Parts Discussed in Thread: SYSCONFIG,

Tool/software:

Hello E2E,

When I use the sysconfig tool to generate the radio command structures I can see RF_cmdPropRx.pktConf.bChkAddress to enable address check and .address0 and .address1 structure elements to set a byte ! (sparingly either one of those?) when the radio receives a packet.

I would expect similar setting on the Tx side as well, I am unable to find any such structure element in Tx section. I checked in the SmartRF Studio generated code as well. I don't see any difference in structures or exported code with enable or disable the address check mark.  

Also I was looking for the PAD ID settings for any Tx/Rx packets. FYI. I am using rfUARTBridge_CC1354P10 stock example as a base for my application.

My intension was to use the CC13xx radio between a remote and receiver to exchange some secure data. Any help would be highly appreciated. 

Regards,

Satya