Part Number: CC1352P7
Tool/software:
Hi!
I am developing hardware using the CC1352P7 to run Wi-SUN. I used the Launchpad LP-CC1352P7-1: 868/915 MHz up to 20 dBm, 2.4 GHz up to 5 dBm as a reference.
I just didn’t include the parts marked in green in my schematic:
Could this cause connection issues?
Below you can see it in my schematic:

(1) I reduced the resistance of R18 to 10K.
(2) I removed the capacitances of X1A (because the circuit couldn’t maintain ifconfig up and wisunstack start).
(3) Now I can keep ifconfig up and wisunstack start, but I can't make my device connect to another.
(4) Using the RF-star module with CC1352P7 connected to my antenna, I achieved a stable connection.
(5) How can I force communication through the 14 dBm differential pair? I want to check if the issue is with the soldering of the “SKY13317-373” chip.
Any debugging tips?
Attached are the copper layer plots of my PCB and also the schematic: