This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312PSIP: Debugging with XDS110 on collector project.

Part Number: CC1312PSIP


Tool/software:

On our design, I am unable to debug only the collector project.  It gets stuck at Can't find a source file at "/home/developer/.conan/data/ti154stack/6.41.00.07/library-lprf/ga/build/c90184d484f3f95c6a6179391966efa64b8ab8fe/build/cmake/ticlang/..\..\..\source\ti\ti154stack\low_level\cc13xx\mac_radio.c" showing macRadioPowerUpWait() at mac_radio.c:1,493 0x16c5a.

Can you tell me why this is happening and if I can get source to this?

Thanks,

Kevin

  • Hi Kevin,

    can you share with me how you have the XDS110 connected?

    Do I understand correctly that you flashed the device with our default collector example? Dis you use for flashing the XDS110 and was it successful?

    How do you try to start the debug session then?

    Kind regards,
    Theo

  • Theo,

    This is on our board not the LaunchPad.  I can debug on the LaunchPad, but with the same firmware not on our board.  I need to determine what it is getting stuck on.  This happens more often than not, but I have had it sometimes get past this.  I use the XDS110 debugger with a cable to program and debug the board.

    Kevin

  • Hi Kevin,

    this almost sounds like a hardware problem since it runs without any issues on the LaunchPad.

    Could you share with me a screenshot of the debug session that you started and the stack where it get's stuck?

    Kind regards,
    Theo