Tool/software:
Hi,
We are doing some research to develop a new version of our wireless sensors.
We'd like to implement private networks with the following requirements :
1) Low consumption for the sensor nodes (battery powered + solar panel 0.3W) in the network, slightly higher consumption for the collector (battery + solar panel 2-5W).
2) Range >50m
3) We need to collect 1 to 2MB every day from each sensor
4) Around 30 sensors in each network
5) Ideally a Sub 1GHz band but also 2.4 GHz could be good (if the range doesn't drop too much in presence of obstacles) . We are concerned about duty cycles for Sub 1GHz.
6) Time synchronization between sensor and collector (ideally 1ms)
7) No problems of latency, sensor can wait until there collector is free to receive data.
We currently use a CC2652P for a PoC with BLE (LE Coded S=8) as protocol and we are quite happy. Anyway we'd like to switch to a free protocol to reduce the costs due the fact we don't need to interface with other BLE devices (the networks are private). Also if is possible we'd like to switch from 2.4Ghz to Sub 1Ghz bands to extend the range (change the MCU is not a problem).
We think that maybe the TI 15.4 stack could fit, but we'd like to have your opinion.
Thanks,
Riccardo