This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-EM-CC1314R10: Host_collector application reports error as "No reset response received after device reset"

Part Number: LP-EM-CC1314R10

Tool/software:

Hi,

In this i had used two LP-EM-CC1314R10 launchpads (one as coprocessor(LP1) and another one as sensor_OAD_offchip(LP2)).

I'm currently using the host_collector executable with collector.cfg in ti154stack_linux_x64_4_40_00_03. I then used the uniflash program to flash the coprocessor hex file in (LP1). After that, I used the Uniflash program to flash the sensor_oad_offchip bin file and the Mcuboot hex file in (LP2). Following that, I launched the executable ./host_collector collector.cfg in the terminal from the path of prebuilt/bin .It results,

No reset response received after device reset
0) ./host_collector(+0x1f74f) [0x58f07481f74f]
1) ./host_collector(+0x1f8ba) [0x58f07481f8ba]
2) ./host_collector(+0x21e45) [0x58f074821e45]
3) ./host_collector(+0x21dcf) [0x58f074821dcf]
4) ./host_collector(+0x1b422) [0x58f07481b422]
5) ./host_collector(+0x1b495) [0x58f07481b495]
6) ./host_collector(+0x19432) [0x58f074819432]
7) ./host_collector(+0x65c3) [0x58f0748065c3]
8) ./host_collector(+0xfc44) [0x58f07480fc44]
9) ./host_collector(+0x4490) [0x58f074804490]
10) /lib/x86_64-linux-gnu/libc.so.6(+0x29d90) [0x7d0707229d90]
11) /lib/x86_64-linux-gnu/libc.so.6(__libc_start_main+0x80) [0x7d0707229e40]
12) ./host_collector(+0x348a) [0x58f07480348a]

Please support us on this to resolve the issues.

Regards,

Manivel M