Part Number: CC1312PSIP
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
There is an option in the TI 15.4 stack under the MAC Advanced section to Enable Duty Cycle. When I do this, it allows me to only set the Duty Cycle Threshold to 10% without suppressing that message. It also indicates this is only available for ARIB-regulation PHYs. Is it possible to set this Duty Cycle Threshold to 60% and is the WB-DSSS PHY type an ARIB-regulation PHY?
Thank you,
Kevin