Part Number: CC1200
Tool/software:
Hello,
I would like to consult a few questions regarding the CC1200:
1、The INVERT_DATA_EN configuration can invert the payload data during both transmission and reception, but the SYMBOL_MAP_CFG should have the same effect. However, it seems ineffective when configured.
2、Can the SYMBOL_MAP_CFG invert the preamble and sync word during both transmission and reception? It seems ineffective when tested.
The transmitter uses the SX1262 RF chip, and the sync word in the TX FIFO is CC CC CC CC CC CC CC CC CC CC ... CC 81, with inversion enabled. However, when the CC1200 receives with the sync word set to 33 33 33 7E, it incorrectly triggers the sync word interrupt.
3、If the CC1200 receiver is configured to not detect the preamble, will this affect its reception performance?
Could you kindly take a look at these issues when you have time? Thank you very much!
best regards!