Part Number: CC1311R3
Tool/software:
Hi,
Customer is making the screen TX power limitation.
the TX power setting is -3dBm.
Could you please share the tx power accuracy under -3dBm setting?
BR. Albin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC1311R3
Tool/software:
Hi,
Customer is making the screen TX power limitation.
the TX power setting is -3dBm.
Could you please share the tx power accuracy under -3dBm setting?
BR. Albin
Hi Albin,
In the PA table for CC1311R3 we don't have a -3 dBm setting. Can you verify which setting they are using? Is it -5 dBm?
Referring to the FCC 15.249, the peak power of 920MHz should be less than -1.25dBm, The output power of the products on the production line is based on a power range, which is defined as the target power ± the power tolerance. I need to determine how to set this power range to ensure all products meet the requirement of being below -1.25 dBm.
-3 dBm is just an example. The actual setting depends on how accurate your power calibration can be. If you can achieve a precision within ±1 dB, I would set it to -2.25 ± 1. If the precision is within ±2 dB, I would set it to -3.25 dBm.
If you can only configure it to the -5 dBm range, please evaluate whether the power accuracy can ensure that all devices on the production line remain below -1.25 dBm.
Hi Qiang,
from characterization data under typical conditions, the -5 dBm setting would remain below -1.25 dBm.