Tool/software:
I need to implement two way communication can possible using cc1101 . currently i am send and receive msg between two module and for that we need to switch rf rx and tx mode . if one device continuos in tx and another second device continuos receive mode and suddenly device second switch to tx for msg send to the device one how to inform device one to switch in rx state. And GDO0 pin how to use for TX transmite and receive interrupt because not undestand the cfgGDO0 config 0X06. please help to implement these.